6/10/2020 8:41 AM | |
Joined: 7/5/2013 Last visit: 9/24/2024 Posts: 3113 Rating: (512) |
Hello System8000, you would need the V11-PLC-project to export proxy-data. Then you can use those proxy-data in the newer HMI-project. Please see Combined configuration with WinCC (TIA Portal) and STEP 7 V5.x or Combined configuration with WinCC (TIA Portal) and STEP 7 (TIA Portel) in separate projects. Or you create just the HMI-project and define the connection to PLC manually. Regards, Frink |
Pi is exactly three! |
|
6/12/2020 10:44 AM | |
Joined: 8/3/2009 Last visit: 9/24/2024 Posts: 13778 Rating: (1740)
|
Hello System800 Here you can see which Kombination from S71200(FW) and Panel IMage Versoin is possible: https://support.industry.siemens.com/cs/de/en/view/109475049 Bye Murof |
Last edited by: Murof at: 06/12/2020 10:44:39If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
6/12/2020 10:45 AM | |
Joined: 8/3/2009 Last visit: 9/24/2024 Posts: 13778 Rating: (1740)
|
Hello Prof. I thought Proxy Data is only supported since V13?? Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on