5/14/2014 1:59 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359) |
Please check the order number in database of online support."ET200S IM151-1" is not a CPU module,check your order number.Even "6ES7151-7AA00-0AB0" doesn't support DP-Master function.I think you need at least Master class1 in your project for communication.
Hope this helps, Hamid Hosseini |
Last edited by: hdhosseini at: 5/14/2014 2:00 PM |
|
This contribution was helpful to1 thankful Users |
5/14/2014 2:23 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello Poljachina What is Node 2 ? Normally Profibus address 2 is the Default address if Profibus Port of CPUs or DP Masters. If this is a CPU with Function Blocks, then the IM151-1 would be configured as a Slave in the CPU Configuration and not the MP277( Which does not have DP master Capabilities. ). In your case the Node-2 ( As you define it ) is probably the CPU and is the Master for IM151-1. MP277 can only communicate with a CPU. You need not define it in the PLC hardware configuration. You will need WinCC Flexible to configure the MP277 . It can be configured as : a) Either as an "Integrated" HMI ( Just insert ) the HMI in SIMATIC Manager ( After installing WinCC Flexible ) and configure it using WInCC Flexible. b) or you can have the HMI as a Stand alone project. You just need to define the CPU Address and Communication type ( Profibus ) in this case to establish communication between the two. Hope this helps Cheers Navnag |
Last edited by: Navnag at: 5/14/2014 2:32 PMThere is no such thing as the last bug in a program |
|
5/14/2014 2:35 PM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hello Poljachina, As Hamid Hosseini explain, Have a look on the Module no. you have in your System. without CPU or ET200S CPU you can able to Communicate with only IM151 not with HMI MP277. If you have a ET200S CPU i.e IM151-7 then You can used the 6ES7138-4HA00-0AB0 DP MASTER INTERFACE FOR ET200S CPU, |
Ammy |
|
This contribution was helpful to1 thankful Users |
5/14/2014 2:39 PM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8612 Rating: (1147)
|
Hello, When you have a MP277 and WinAC MP, (soft PLC on panel), you can connect ET200S (IM151-1) to MP277. But the WinAC MP is declared mature product, see the following link: SIMATIC WinAC MP 2008 Declared Mature Products Best regards, Wizard |
This contribution was helpful to2 thankful Users |
5/14/2014 7:03 PM | |
Posts: 62 Rating: (0) |
Yes this has to be installed on the MP277, or is this this software package installed on the PC? |
5/14/2014 9:06 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello Poljachina What Wizard has suggested is an interesting possibility ( Though it was not very popular ). Does this mean that the Node-2 reffered by you in the MP277 itself. The Software Package referred by Wizard has to be installed in the MP277 and not in PC. Just check out this Delivery release for WinAC MP 2008 software PLC WinAC MP 2008 can be downloaded from here Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on