7/28/2016 6:46 AM | |
Joined: 5/6/2010 Last visit: 4/24/2024 Posts: 1963 Rating: (272) |
Hello, if you use TIA please look at this article: This should solve your problem. regards |
7/28/2016 9:12 AM | |
Posts: 3 Rating: (0) |
Thanks for the answers The problem is that the ET200SP does not support "pack addresses". Do you know another solution? Thanks
|
7/28/2016 9:19 AM | |
Posts: 1529 Rating: (202) |
Leave them as 4 bit addresses. Is this a problem? Are you running out of addressable I/O? |
7/28/2016 9:52 AM | |
Posts: 3 Rating: (0) |
Yes it's a problem. This is an existing installation with existing schemas. Only the PLC is changed.
|
7/28/2016 11:19 AM | |
Posts: 1529 Rating: (202) |
Then don't use SP. Use S instead. |
8/2/2016 9:40 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi, Address packing is not possible with ET200SP. see this previous post: Address packing on ET200 SPhope this helps, regards, |
FCK WAR! |
|
Follow us on