10/20/2007 9:17 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Hi, If you built up the hardware and project there the analog outputs as redundant set then it must work. Please consider that you have to place the software between the redundant software blocks for reading in and writing out the redundant I/O. So the software to write the analog output must be between those blocks.... and only write the lowest word with the value you want. Is there a passivated signal ? |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
11/2/2007 6:42 AM | |
Posts: 8 Rating: (0) |
Hallo, Thanks for ur reply. I need help on S7 400 H system with IO redundancy. I am facing problem with Analog Output modules. I don't have documents giving information about its configuration and use. Can U please tell me the linkwhere i can get sample program and documents |
11/8/2007 7:49 AM | |
Joined: 9/27/2006 Last visit: 4/18/2024 Posts: 12256 Rating: (2664) |
Hello prash; The manual for the S7-400H system can be downloaded here: http://support.automation.siemens.com/WW/view/en/1186523 There is a chapter on I/O configurations, including redundant I/O. The following FAQ discusses the use of I/O edundancy on the S7-400H. http://support.automation.siemens.com/WW/view/en/9275191 Hope this helps, Daniel Chartier |
12/17/2007 4:23 PM | |
Posts: 8 Rating: (0) |
Hi Late, Thank you very much for your help. Regards. |
12/17/2007 4:30 PM | |
Posts: 8 Rating: (0) |
Hello dchartier, I downloaded manual from the link provided by you and could configure the S7-400H System. Thanks for ur help and support. [snip] ... |
Last edited by: CS Moderator at: 30.12.2007 00:32new question splitted to a seperate thread /tf/WW/en/Posts/14390 |
|
1/10/2008 10:12 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Dear Prash, Thank you, are you now have a working H-system with redundant analog I/O ? |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
8/3/2009 9:45 AM | |
Posts: 2 Rating: (0) |
Hi everybody. I have the sam problem and I couldn't solve that. i read the manual file but it can't help me. has anybody a sample code? Thanks alot |
8/3/2009 5:42 PM | |
Posts: 51 Rating: (4) |
Hi all,
I have same problems with using AO card 332-5HD01 and using FB451. I tested many ways , when I use FB451 the system fails and error is Area Lenght Error when reading/writhing. I could handle redundant AI modules but AO doesn't work. some times it works but when I remove second module and insert it again the current is not halved and total current is on the module with lower address. also I removed module,waited for depassivation and inserted it again and after insertion that error occured. also AO is sensitive with removing AI. can anyone help me? regards. |
9/4/2009 1:00 PM | |
Posts: 12 Rating: (0) |
dear pioneer, i am also searching for how to configure redundant i/o signal. do you have any sample program for redundant AI and AO signal programming. can you tell me how to configure AI redundant signal. regards, senthl |
Follow us on