Industry Online Support
Technical Forum
4/2/2011 4:34 PM | |
Posts: 3 Rating: (0) |
Dear pouya, I use PCS7 Ver 6.1 with Step 7 ver 5.4 to configure im153-2 (2BA02)hardware..Of course it work well when using PLC but when i used PCS7 (CFC + SFC) i'm facing a lot problem with my software...DO signal cannot been produce...What is your solution for your project...is it you do upgrade PCS7 version by using Ver 7....?? rgds RUKU Splitted from I tried to add this this new IM 153-2 to my Hardware Configuration catalog, but I could not. |
Last edited by: O_Moderator at: 4/5/2011 10:01 AMnew subject after splitting |
|
4/2/2011 4:58 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
OFFTOPIC Is not recommended to update Step7 version in case of PCS7. The rule there is to update PCS7 using corresponding SPs or updates. The second point is to take in mind PCS 7 V6.1 Released Modules. (for example). Each version of PCS7 has its corresponding released modules. Of course is possible to install GSD file but after you should manual prepare the software. |
4/5/2011 10:05 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already discussed in the following thread configuring im153-2 (2BA02)hardware. Best regards O_Moderator |
Follow us on