Industry Online Support
Technical Forum
4/2/2014 4:36 PM | |
Joined: 2/24/2014 Last visit: 8/31/2023 Posts: 1 Rating: (0) |
hi daniel, right now we are trying to configure RX3i system with im-153-2 (DP/PA Link) and FDS 157 as DP/PA coupler, with E+H liquiphant as slave right now i able to made the GSD file with gsd tools as attached, while configuring in RX3i, under profibus master we add IM-153-2 as slave, and we add module: 1. Begin of Device_152, with parameter of 3 (HW address of liquiphant) 2.== Discrete In_152B, this will will create BF1 flahing red and BF2 red lamp is on in IM3-2 but if we remove module "begin if device_152", and only use module "== Discrete In_152B", BF1 will remain off and the communication to GE profibus card is established,but the BF2 in IM153-2 are steady on "red" would you mind to help to adviced on this? many thank's Attachmentsip58052 - Notepad.pdf (174 Downloads) |
Last edited by: CS Moderator at: 4/4/2014 10:49 AMnew subject after splitting from /tf/WW/en/Posts/18942#top |
|
Follow us on