10/2/2015 8:02 AM | |
Posts: 1 Rating: (0) |
hello, i have a problem in configuring the CP 243-1 ethernet module .when i add this module through wizard. mpdule cannot be read.IN tutotorial i saw the video in when the tutor click on the read module the module location and model are shown .the is given below . any one help me what can i do . ------------------------------------------------------------------------------------------ Attachmentuntitled.rar (150 Downloads) |
Last edited by: mofadun at: 10/2/2015 8:04:16 AMLast edited by: mofadun at: 10/2/2015 8:05:12 AMLast edited by: Min_Moderator at: 10/2/2015 1:15:34 PMNew subject after splitting |
|