3/19/2013 5:14 PM | |
Joined: 12/19/2011 Last visit: 9/4/2024 Posts: 36 Rating: (0) |
Hello! I have a cnc 840Dsl NCU710.2. Installed on the machine spindle gearbox ( motor - gear - sensor - gear - load). Each gearbox switches to two positions. Spindle has 4 ranges. The Problem is that the sensor is mounted on the intermediate shaft of the gearbox, and the reduction of the sensor and the motor or spindle, varies depending on the specified range.In the parameters of the CNC is the parameters for a single measuring gear (with a constant gear ratio).Engine without the sensor, install the sensor in a different place is not possible.Please help solve this problem.
Attachment111.pdf (401 Downloads) |
Last edited by: spec-cnc at: 3/20/2013 9:12 AMLast edited by: spec-cnc at: 3/19/2013 7:00 PM |
|
3/20/2013 6:59 AM | |
Joined: 3/19/2006 Last visit: 4/29/2024 Posts: 594 Rating: (78) |
What do you mean sensor ? encoder or proximity switch
|
3/20/2013 8:31 AM | |
Joined: 12/19/2011 Last visit: 9/4/2024 Posts: 36 Rating: (0) |
I have installed an encoder |
3/22/2013 10:50 AM | |
Joined: 12/19/2011 Last visit: 9/4/2024 Posts: 36 Rating: (0) |
Hi! Thank you for your response. 1. I set the parameters for each range of spindle MD31050 $ MA_DRIVE_AX_RATION_DENOM MD31060 $ MA_DRIVE_AX_RATION_NOMERA I can not set the parameters MD31070 $ MA_DRIVE_ENC_RATION_DENOM MD31080 $ MA_DRIVE_ENC_RATION_NOMERA because they set a constant reduction. I have two different reduction to four bands of spindle 2. I do not have spindle orientation and no switch on the spindle. Thank you again!... Attachment222.pdf (389 Downloads) |