6/11/2011 4:21 PM | |
Posts: 691 Rating: (36) |
Hey fritz Your way of explaining made you this far. |
This contribution was helpful to1 thankful Users |
6/11/2011 9:22 PM | |
Joined: 8/25/2006 Last visit: 4/26/2024 Posts: 2203 Rating: (277) |
Hello. You forgotother platin experts. E.g.: Gebhardt Karl, Late, J_Bell, Wizard, Phantom75. |
Last edited by: KSN at: 6/11/2011 9:24 PM |
|
This contribution was helpful to2 thankful Users |
6/12/2011 12:02 AM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Dear Fritz, First I must congratulate you for your 2nd platinum brick. Nothing to say but really well deserved. ----------------------------------------------------------------------------------------------------------
I just see that two of the very best experts have been missed so I decided to make a list of all platinum experts we do have in our forum and for sure we all learn from them. Aret dchartier(2 platinum bricks by the way) fritz Gebhardt Karl J_Bell Late Phantom75 UMENCHO Wizard In addition here come the platinum expert (considerably). IBN-Service Best regards. H-H |
This contribution was helpful to4 thankful Users |
6/12/2011 2:07 AM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
I mentioned OTHER platinum also... ANy ways thanks for adding all names.... Hope in Next Campaign we can see all of these in Diamond Club and some of these even at the Level to cross Diamond and reach next level.. |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to1 thankful Users |
6/12/2011 1:08 PM | |
Joined: 10/7/2005 Last visit: 4/26/2024 Posts: 3004 Rating: (1046) |
Dear all my initial thoughts upon reading IBN-Servicepost were: “Out of all the odd and quirky threads that were started during this Premium Campaign, this one surely is up there with the most bizarre ones”. Then I quickly realised two things: 1.)It was IBN-Service who wrote the original post and - put in that context - the entry all of a sudden appeared rather normal. 2.)He had only two spaceholders in the “Kicking you’re a**!”” post heading instead of three.As such, should you dear Juergen do have the chance to come Down under one day, I try to organise a donkey so you can live out your secret fantasies (I presume that the “**” represent an “s” each and the Oxford English definition of thisis: “a hoofed mammal of the horse family, which is typically smaller than a horse and has longer ears and a braying call”.) For the record, I am against all forms of Animal cruelty, so it will have to a plush toy donkey for Juergen to kick (I shall upload some pics here of the event if and when it takes place). On aserious note, I thank all of you for your kind words, they are much appreciated. |
Last edited by: fritz at: 6/14/2011 9:57 AMThis entry may not make too much sense anymore since the Moderators decided to merge the thread that IBN-Servcie started (titled "Congratulations fritz, I''ll be kicking your a**") with this thread. I didn''t ask for it and wish they wouldn''t have, but so be it (its not the end of the world either). Cheers |
|
This contribution was helpful to9 thankful Users |
Follow us on