9/2/2019 2:31 PM | |
Joined: 2/4/2015 Last visit: 6/18/2024 Posts: 64 Rating: (0) |
Dear Sir, I want to connect 120 nodes(IMCC) via single profibus master. I planned to use 3 RLM(Redundancy Link module) and 40 nodes in each RLM. Is it possible? I have read that maximum 32 nodes per segment. Can it be increased by using repeaters. I have attached my proposal. I want to use 1.5 MBPS. Kindly suggest. Surendhar M ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/03/2019 10:11:08New subject after splitting |
|
9/3/2019 11:27 AM | |
Joined: 2/4/2015 Last visit: 6/18/2024 Posts: 64 Rating: (0) |
Thank you sir. I hope the same is applicable to Siemens by using Y Links. Surendhar M |
9/3/2019 1:13 PM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello Surendhar; I am not completely familiar with the RLM01, so I cannot discuss the inherent limitations of these modules without further study or assistance from ABB (which I suggest you consult for this type of network design). I know the Y-links though, and can discuss the limitations they would impose on your project. SIMATIC Bus links DP/PA coupler, active field distributors, DP/PA Link and Y Link https://support.industry.siemens.com/cs/ww/en/view/1142696 As you can see from the technical specs of the Y-Coupler (one element of the Y-Link) below, you are allowed to have up to 64 slaves on a Y-Link, using repeaters (OLMs are acceptable to, for fiber-optic connection).So far it looks good for your design. However, the Y-Link is considered by the redundant CPU masters (H-system) as a single Profibus-DP slave, and as such follows the limitations of a single Profibus slave: the amount of data to be exchanged with all of the configured underlying slaves on the Y-Link is limited to 244 bytes OUT/244 bytes IN, no matter how many underlying slaves it connects to the redundant masters. So each of your 40 slaves on a Y-link (with repeater to control more than 32 nodes) would each be limited to 6 bytes OUT/6 bytes IN on average, on each Profibus cycle. Is that enough for your project? Another limitation is the 244 byte parameter assignment frame for the slave, less known but that can cause problems when you have so many underlying slaves. There is no warning that you are approaching this limit, only that you have overpassed it and that the slaves cannot be configured when you do. So be very careful before actually committing to using Y-Links on the project, and I would carefully evaluate any other type of link from other vendors. You could also get help from a Siemens rep, or come back to the forum when you have advanced your network design Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 09/03/2019 14:57:42 |
|
Follow us on