1/22/2017 12:40 PM | |
Joined: 9/9/2015 Last visit: 5/10/2024 Posts: 727 Rating: (268) |
I was trying to connect Aggr1FP - IN(ANY) directly to the MotSpdCL RdyToStart Output (Struct) in different CPU by using AS-Wide Interconnection, but eventually, the error (254:61040) popped out. When I tried to connect to out data type such as real, bool across PLC, there had no such error code. Could any one let me know how to connect Aggr1FP to another CPU out in order for me to call the Faceplate in the HMI? Thanks. Details of the System. Both of the CPU are using H-systems CPU410-H and PCS7 V8.2. AS Oriented Multiproject. . ------------------------------------------------------------------------------------------ AttachmentScreenshots.zip (53 Downloads) |
Last edited by: Min_Moderator at: 1/23/2017 3:18:24 PMNew subject after splitting Please give me 5 stars Rating if my post is helpful for you. :) |
|
3/25/2017 7:08 AM | |
Joined: 9/9/2015 Last visit: 5/10/2024 Posts: 727 Rating: (268) |
My temporary solution for this thread is adding a Intlk02 block in CPU A in between of the aggr08(In CPU A) and spdCL (in CPU B). The reason im doing this is the input of Intlk02 allow AS-wide connection and most importantly is, i could like faceplate with this method. By the connection above, when i call the faceplate in WinCC using aggr08 standard faceplate, i will be linked to intlk02 faceplate first. Then, i can click on the Intlk02 faceplate jump button to jump over to the SpdCL faceplate. This is my temporary solution and it is very stupid. I will seek siemens's advice to solve the SelFP input issue. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
3/28/2017 9:24 AM | |
Joined: 9/9/2015 Last visit: 5/10/2024 Posts: 727 Rating: (268) |
There are one note of AS-wide interconnections: STRING, STRUCT, ANY and POINTER data types are not supported. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on