4/8/2019 3:23 PM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello AutoGen_7464634, I'm not a PH/IS expert. I can only give you the advice to check the application example Installation, Operation and Maintenance of Process Historian/Information Server in a PCS 7 Environment. With regards |
This contribution was helpful to1 thankful Users |
4/8/2019 4:27 PM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Dear Autogen, I have no experience in installing them in the same stations. But you could verify whether can they be installed in the same station or not. Will the SQL crash each other? Normally i separate WinCC and IS. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
4/10/2019 4:16 AM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
Dear Autogen, From the manuals, it said WinCC and IS can be installed together but WinCC has to be the first one. Can you confirm this? If necessary, try to use a clean copy or different environment to set this up again. System.ServiceModel.Channels seem related to .NET items. Can you make sure your IIS is installed? Page 11, Installing IIS for Window 7 SP1. (I'm referring to Information server SP3) May be you can try session 1.2.2.3 Installing Visual Studio Tools for Office (VSTO Runtime) Install the Microsoft .NET Framework 4.5.1 as well . Make sure IS ready is installed up to the latest version. You need IS ready to communicate with IS. And lastly, my recommendation is to disconnect Wifi, make sure your station is using static IP instead of dynamic. I faced quite a lot of issues with wifi connected before. Just a recommendation. |
Last edited by: Jen_Moderator at: 4/10/2019 9:31:51 AMOptimized link. Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on