4/13/2016 9:10 PM | |
Posts: 25 Rating: (0) |
[snip] Another question; is it possible to connect os reference to AS directly with cp1623, or is reference will get data from os base? ------------------------------------------------------------------------------------------ |
Last edited by: Rozen at: 4/13/2016 9:10:40 PMLast edited by: Min_Moderator at: 4/14/2016 10:59:44 AMNew subject after splitting Last edited by: Min_Moderator at: 4/14/2016 11:01:05 AMSplit from other thread |
|
4/14/2016 9:02 AM | |
Posts: 25 Rating: (0) |
Dear friends Thank you very much. Could you tell me more about os single station redundancy configuration. |
4/14/2016 9:45 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Hi Rozen, You can configure two single stations as master and standby. In runtime, when one server fails, the other one will take over and you still have visualization. In order to do this, you have to configure one single station with: "WinCC Application". The other station is configured as "WinCC Application (Standby). On the OS properties of the standby server, you can set the target computer and also set the master server. In this case, you can configure the master server and the standby is just a copy of it. You have to do some more work like redundancy settings. I have a few links, where everything is explained further. In the PC configuration document, you can see which solutions there are with Single Stations. Engineering Station (V8.1 SP1) |
Last edited by: Oreca at: 4/14/2016 9:50:12 AMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on