6/26/2017 11:26 PM | |
Posts: 1 Rating: (0) |
Good afternoon, I am Pablo, from Ecuador, do you know if it is possible to connect RTD with 3 wires directly to analog inputs in PLC S7 1200 AC / DC / RLY? I know analog inputs suport 10 VDC, but I have 24 VDC source, what can I do to get only 10 VDC? I gonna to use a voltage divider, but I'm not sure if it's a good idea.
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/27/2017 10:41:25 AMNew subject after splitting |
|