Industry Online Support
Technical Forum
8/20/2015 7:54 AM | |
Joined: 7/25/2013 Last visit: 10/24/2023 Posts: 4 Rating: (0) |
I try to connect s7-1214c v4.1.1 6ES7 214-1AG40-0XB0 and IM153-4 v4.0.3. PLC is not transferred to the run, IM153 s blinking frequency of 1 per second. The status says "Not reachable Differences were found between the loaded configuration and the offline project. Online article number:? Offline article number: 6ES7 153-4AA01-0XB0 ". Changed module IM153-4 to v3.0.0 - did not help. I think the problem is in the PLC. Change it, or to update the firmware to 4.1.3. May be try to find 6ES7 214-1AG31-0XB0? IP address PLC 192.168.0.11, ET200M IM153-4PN - IP address 192.168.0.9 ------------------------------------------------------------------------------------------ |
Last edited by: ugpromavt at: 8/20/2015 8:07:46 AMLast edited by: ugpromavt at: 8/20/2015 8:55:03 AMLast edited by: Min_Moderator at: 8/20/2015 11:16:21 AMNew subject after splitting |
|
Follow us on