4/23/2018 10:23 AM | |
Posts: 2 Rating: (0) |
Hello, I need to connect a PLC S7-200 (CPU 214) with a simatic panel touch tp270. I have no idea which cable to use, any one of you can help me? |
4/23/2018 1:40 PM | |
Joined: 3/28/2015 Last visit: 5/4/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topic might help: |
Eng.Mohamed Ibrahim |
|
4/23/2018 1:46 PM | |
Posts: 2826 Rating: (684) |
Look at the sections mentioning connections in the manual -> The connection between TP and PLC is a coper cable. Between PC and TP can be the PPI cable you use for programming the S7-200. |
Follow us on