4/27/2019 8:06 AM | |
Joined: 11/29/2018 Last visit: 7/1/2024 Posts: 1 Rating: (0) |
Hello dear zackk0! I have a question: in general, I wanted to connect the Profibus PA device to the s7-1200. At first I tried to connect DP / PA-link with s7-1200. But it does not work. I did everything I could. GSD file generated using gsd_tool: sip58052.gsd Please tell me how you configured and what parameters were configured on the TIA portal. And one more question: did the devices appear with Profibus PA? And How? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/02/2019 14:55:16New subject after splitting |
|
5/2/2019 3:33 PM | |
Joined: 9/27/2006 Last visit: 9/20/2024 Posts: 12282 Rating: (2684) |
Hello kamal; It is very difficult to provide help if the only information you provide is "it does not work". First, what version of Step 7 are you working with? What is the DP/PA link configuration you want to integrate? What error messages do you see? Could you attach the gsd file that you generated, along with a list of instruments you want to connect to Profibus over the DP/PA link? Did you follow all instructions to generate the gsd file from this FAQ? "Copy the GSD files of the PA slaves into the "gsd tool" directory. In the "gsd tool" directory you double-click the "gsd-tool.jar" file to start the GSD tool. How do you configure the DP/PA link in the external master or in STEP 7 (TIA Portal)? https://support.industry.siemens.com/cs/us/en/view/79159361 Hope this helps, Daniel Chartier |
Follow us on