Industry Online Support
Technical Forum
9/13/2011 3:12 PM | |
Posts: 344 Rating: (50)
|
Can you ping the IP address of the Simotion controller your are trying to access? Simotion has a build-in web server. Can you access that from web browser? |
9/13/2011 8:33 PM | |
Posts: 344 Rating: (50)
|
The next thing is to check programing device settings (PG/PC) in NetPro (attached picture). The Scout project needs to know which port on Simotion controller, IP Address and Ethernet card in the PG/PC is used to connect to the Simotion controller to figure out the appropriate routing. Also, take a look at this FAQ for connecting to Simotion via a Scalance router for additional help on settings. |
9/15/2011 11:39 AM | |
Posts: 487 Rating: (36) |
The setting should be right because when I use the project on our internal network , it works ,connection is ok .it must be something specific to using a VPN connection. We checked the document on the faq : https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=26662448&caller=view and opened the proper ports and allowed for the various protocols |
9/15/2011 4:33 PM | |
Posts: 344 Rating: (50)
|
Is the Simotion controller setup in the project to send the response back to the router gateway? |
9/16/2011 9:20 AM | |
Posts: 487 Rating: (36) |
Denis Yes router adress is included and works ok . Thanks for your assistance so far . Eric |
Follow us on