Industry Online Support
Technical Forum
2/2/2010 8:11 AM | |
Joined: 10/7/2005 Last visit: 9/22/2024 Posts: 3021 Rating: (1054) |
Hello adilmahsan I'm afraid to tell you thatI think you are out of luck. The only way to connect any the latest/current Panels (all that end with a "7" in the part number) to an S5 is via Profibus DP. What you however asked for and need is the ability to connect to the AS511 programming port (and you can't even get a Profibus DP card for your 100U as an alternative). Should not have yet bought the TP177 you could try to get hold of (a superseeded) TP170which you can conect to the AS511 programming port (in which case you can find more infoon connection cables HERE). If you already have the TP177 you may be better off upgrading the S5 to an S7. I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on