6/19/2014 9:04 AM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711) |
Hello, you need to use OPC to connect the 1200 to Wincc 6.0. How do you connect a PC station to an S7-1200 with OPC? Regards, Marcjan |
Problem solved? |
|
6/19/2014 10:55 AM | |
Posts: 49 Rating: (9) |
Hi, Another option might be the Modbus TCP connections BR. Ghassan
|
6/19/2014 11:46 AM | |
Joined: 6/18/2014 Last visit: 8/18/2022 Posts: 7 Rating: (0) |
Hi, Thx, but can you please help me a little more? I'm stuck on chpter "6 - compiling and downloading the pc station configuration". I've followed the previous points using TIA portal that is installed on another PC. now trying to compile and download the pc station to the pc that only has WinCC 6.0 SP4 installed I don't know what to do. First I don't have "Station Configuration Editor" in the WinCC 6.0 PC. Is that a software I can download somewhere? I'm stuck on this :s |
Follow us on