1/12/2009 8:36 AM | |
Posts: 62 Rating: (2) |
Hi rambiz, |
1/12/2009 9:42 AM | |
Posts: 4 Rating: (0) |
hi again, i'd like to have them as server/client. regards |
1/12/2009 10:00 AM | |
Posts: 62 Rating: (2) |
Hi rambiz, No need toconfigure any driver or channel, because basically client accesses to server viaserver data package. Usually, at thesever youconfigure as multi-user project andlet the client accesses to the server by using SIMATIC-Shell.There are a lot of relevanttopic in FAQ e.g. http://support.automation.siemens.com/WW/view/en/22132850 Regards, Yai |
1/17/2009 1:15 PM | |
Posts: 4 Rating: (0) |
hi all, 1. if i try to open the project through WinCC Explorer,i see the project on the server but if i try to open it, it doesn't ask me for the user/password of theclient and i get the usuall prompt: I have to add that the client doesn't seem to have access to *.mdf and *.ldf files, 2. when i explore the folder WinCC Projects on the client (My computer ---> WinCC Projects),i don't see the server (John) under 3.the 3rd method, namely using "autostart" doesn't work either although this time i at least was promted to enter the username and passwordfor the client, which was not the case for the first method. i have Attachment2ndWay.zip (53 Downloads) |
1/19/2009 9:35 AM | |
Joined: 4/5/2006 Last visit: 9/16/2024 Posts: 917 Rating: (63) |
Hi rambiz, a queston at first: what WinCC version are you using?
You need configure computer into WinCC project with same name of your computer Windows where you are opening it. did you seen this link about Hresult? http://support.automation.siemens.com/WW/view/en/23711489
I suppose you have more than oone network if you are using wireless. Did you selected the right network card into your WinCC projects with right network address? (right click, properties...) Dependig from version are you using should you go into "My Network place" properties, "Advanced" menu, "Advanced Setting" and move your wireless card on the top of list. At the end...just to be clear, you talked about 3 methode...well..are not methode but you need all 3 operation to make your project works. Hope can help Regards |
Follow us on