12/29/2018 10:50 PM | |
Posts: 3 Rating: (0) |
Hello to everyone, I´m a bit new in all this configuration world...so please bear me. I have tried to follow the manual and everything goes well until I try to download the hardware and software to the PC Station (page 28 in the manual). When I try to download it, the IE_general doesn´t show up. I attach some screenshots so that it is easier for you to check what I am doing wrong. I don´t know what else to try... I am using a PLC 1211C DC/DC/DC and a virtual machine with TIA Portal V14 SP1 Update 5. Thank you very much in advance. Carlos ------------------------------------------------------------------------------------------ AttachmentOPC_Communication.docx (97 Downloads) |
Last edited by: CS Moderator at: 12/30/2018 11:51:29 PMNew subject after splitting |
|
1/6/2019 8:42 PM | |
Posts: 3 Rating: (0) |
Hello Murof, You were right, I imported the xdb file and I was able to download the configuration to the PC Station. However, when I continue with the manual and try to create the OPC items in the OPC Scout, the server doesn´t show up. I attach some screenshots so that you can see what I am missing. Thank you very much in advance. Carlos AttachmentOPC.docx (81 Downloads) |
1/6/2019 9:30 PM | |
Posts: 3 Rating: (0) |
Okey, I have done it. It was under the folder \SYM. It works. :) |
Follow us on