8/7/2013 6:37 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Farhan Hi vajont Can you post the Pin details of H51q-HRS ? Normally the RS485 Connection requires you to connect only R(A) and R(b) + Shield ( and Ground - if available ). Pl see the typical connection details. You don't need to connect T(A) , T(B) if you are using RS485 2-Wire conection. Pl seet attachment for a typical RS485 2-Wire connection for CP341 Hope this helps Cheers Navnag AttachmentCP341_RS485_2Wire.pdf (921 Downloads) |
There is no such thing as the last bug in a program |
|
8/7/2013 7:44 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hi vajont You should be able to test communication with CP341 using any RS232 to RS485 convertor. Use a Modbus Master / Slave Simulator on your PC for testing : http://www.modbustools.com/index.asp Please check that you have made the correct settings in the CP-341 hardware configuration ( After installing CP-PTP software ) and the Blocks in STEP7 software have been called properly. If you can upload a copy of your program then I can have a look at it . Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
8/7/2013 9:05 AM | |
Posts: 7 Rating: (0) |
DearNavang simple program hat i use for communcation for get a word with adress zero slave number2 please see that thanks and regards farhan
AttachmentCP341_Ma.zip (306 Downloads) |
Follow us on