10/27/2008 9:53 AM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello Ayman; If this can help, here is part of a document we used a few years ago when we needed to interface a Simatic G150 to Controllogix and GE Fanuc PLCs using Profibus-DP.
You need to use the Delta V Profibus configurator (Sycon, I believe) to integrate the drive gsd, insert a drive on the configurator's bus, create a link from the master to the drives (select the correct Profibus address for the driveand selectmodules with appropriate I/O addressing); then the drive has to be parametrized to give you access to the correct telegram and values. There are a few "standard" telegram formats available for the G150, and telegram 999 is freely configurable. You must ask the technician setting the drive parameters to select the telegram number in P0922, then set the registers you want to read for each of the available addresses in the input telegram; you see above the values we chose and their associated registers in the G150. One thing is that we did not use the OUT addresses to send commands to the drive, the client prefered hardwired signals, so you will have toresearch that part. You should take a few minutes to study the Sinamics G list manual, you will find informative function diagrams for Profibus connections and telegrams. http://www.mawos.com.pl/Files/SING150_LP_EN.pdf Hope this helps, Daniel Chartier |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Last edited by: dchartier at: 10/27/2008 9:57 AM |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
4/1/2015 3:47 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
4/21/2016 2:10 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by mustapha81 is split to a separate thread with the subject Problem with emerson AMS DEVICE MANAGER 11.1. Best regards |
Follow us on