5/25/2014 1:39 PM | |
Joined: 9/16/2011 Last visit: 9/10/2022 Posts: 291 Rating: (6) |
As very well explained byhdhosseini.it is simply driver problem, but for my knowledge like to ask, Can you see you usb-serial convertor as a hardware in youw windows7 device manager. just check it out. |
Reg, |
|
5/25/2014 1:46 PM | |
Posts: 54 Rating: (0) |
The USB-SERIAL converter is working fine with many other devices. Only on STEP7 I have this problem
|
5/25/2014 1:52 PM | |
Posts: 784 Rating: (52) |
I install the software for converter USB/RS232 in Windows 7 and it appears in thedevice manager as serial COM. |
5/25/2014 1:55 PM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359)
|
Perhaps you need to follow the steps shown in the attachment, as my converter is connected to my system. Also check PG/PC interface! AttachmentHD_PORT.zip (624 Downloads) |
5/25/2014 2:10 PM | |
Posts: 54 Rating: (0) |
In the PC/PG Interface i don't have the "local connection" tab. In the HELP it says that it is only for 32-bit systems
|
5/25/2014 2:12 PM | |
Posts: 784 Rating: (52) |
This is the problem. |
Follow us on