6/19/2008 10:24 AM | |
Posts: 78 Rating: (3) |
Hi Eric, Thanks, well, firstly, I configured Unsigned 16bit value, DB10,DW0. and about the connection, as I said before, I'm using AUI to AUI cable, and also I have one tranceiver, can I use it or not?? is there anyway that I can check the connection is correct or not?? about the ping, I don't know, how you can do it? I think Wireshark is good program to show the problem, I hope someone help me how can I use it?? regards, /Alfie |
6/19/2008 10:32 AM | |
Posts: 487 Rating: (36) |
Hi With the TCPIP protocol you give your com card an IP adress , you can then ping this adress with ISO/TF you connect the com cards together using mac adress ( and TSAP).I don't know if you can 'ping' a mac adess.Never heard of wireschark before so , can't help you there Eric |
6/19/2008 10:46 AM | |
Posts: 78 Rating: (3) |
Dear J_Bell, because I didn't have 2 transceivers, so I used AUI to AUI cable instead, ( I asked it in my first post!!) this cable connect to AUI connector (DB 15) from CP1430 to CP1613! ( this link) and would you please explain more about RJ45 to 15pin cross cable?? how can I obtain it? Thanks, Regards, /Alfie |
6/22/2008 1:58 AM | |
Posts: 5822 Rating: (412) |
Dear Alfie, you are right I misplaced RD and TD, but you found it. I am happy that it works now. Best regards J_Bell |
Follow us on