1/12/2016 4:50 PM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684)
|
Hello asd; What model of the Prowirl F 200 do you have in hand (or do you plan to order)? The Endress & Hauser site has a technical information document on this flowmeter that states it can be read out through these interfaces:
The measured values are written from the automation system to the measuring device via the HART protocol. The pressure transmitter must support the following protocol-specific functions: • HART protocol • Burst mode
The measured
values are written from the automation system to the measuring device via the current
input.
The measured
values can be written from the automation system to the measuring via: • PROFIBUS PA • FOUNDATION Fieldbus All of these connections are available with a S7-400H system; I am more familiar with Profibus-PA. For this fieldbus you would have the type of redundant connection shown in the attachment, explained in the following manual: SIMATIC Bus links DP/PA coupler, active field distributors, DP/PA Link and Y Link https://support.industry.siemens.com/cs/ww/en/view/1142696 For hardware: To setup the redundant DP/PA link, you would require 2 x IM 153-2, 1 x DP/PA coupler FDC 157-0 (at least, depending on the number of Profibus-PA buses you want to run), and various active bus modules (models IM/IM and FDC) along with a special mounting rail for the active bus modules; these items are described in Appendix 2 of the manual. For software: To configure and monitor the parameters of the flowmeter you would need PDM software (E&H proposes their Fieldcare package as an alternative); if using PDM, a Basic licenmse will be enough for monitoring uo to 4 instruments: If you decide to use another connection type, tell us so we can give you more information; note that in all cases you will need extra hardware/software. As far as the WinCC display of monitored values, it would be very easy to add a tag and a Output Field in a WinCC page, once the values are input in the PLCs. We can discuss that later. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/12/2016 4:51:59 PM |
|
1/13/2016 8:52 AM | |
Posts: 11 Rating: (0) |
Dear Mr. Daniel, Thank you very much for your support, May I have your email address. Regards, ASD |
Follow us on