Industry Online Support
Technical Forum
3/10/2009 5:54 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello Look at http://support.automation.siemens.com/WW/view/en/13283804 It is made for ProTool, but can also be used for set the WinCC flexible interface. Or just set PG/PC interface to PC-adapter (MPI) instead of (AUTO). After that this link is interesting:Operating S7-PLCSIM through WinCC RT regards |
3/14/2009 7:56 PM | |
Posts: 2 Rating: (0) |
hello, thanks for the help but unfortunately I didn't succeed in solving the matter. http://support.automation.siemens.com/WW/view/en/13283804 : with this link I have put S7ONLINE(Step7)->PCAdapter(Auto), but it doesn't work. then I have tried with PC-adapter (MPI) instead of (AUTO) but the same result. I have also tried to follow the instructions of Operating S7-PLCSIM through WinCC RT, but I'm not able to find Siemens.S/WSPanel.1 in my wincc: it looks very different from the pictures. BR scpr |
Follow us on