8/2/2019 1:10 PM | |
Joined: 5/8/2019 Last visit: 12/28/2020 Posts: 5 Rating: (2) |
Hello to everyone. This is the first time I'm using WinCC, and I'm having problems to connect my PLC to WinCC. I've done a simple program in TIA Portal 15 and upload to the CPU 1212C DC/DC/DC; the IP is 192.168.1.208 and the program is as simple as this: %M0.0 %Q0.0 ----||---------------()- Now I'm triying to create a button in WinCC, and when I click on it the output should be activated. The problem is with the connection, it says "connection status: deactivated" (please, find a picture attached). When I ping 192.168.1.208 in the Command prompt there're no problems, but in WinCC I don't know how to connect the PLC. I've followed this video steps, https://www.youtube.com/watch?v=tKqG1Hgbt4s, but I must be missing something. Can you help me, please? Thanks in adavance.
|
Last edited by: Jen_Moderator at: 08/05/2019 08:21:59Embedded video. |
|
Follow us on