2/18/2013 9:54 AM | |
Posts: 20 Rating: (0) |
Dear experts, how to connection Sinamics - Display(HMI) - Simatic S7-300?and how wiring diagram connection it? used MPI, ethernet or Profibus. Thanks. |
2/18/2013 11:21 AM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, Which Sinamics do you wanto to use? With Sinamics S120 / S110 its no problem, with G120-2 there is no possibility for a direct communication. You can use Ehternet and Profibus- fot a MPI connectioni am not not sure but i think it could work too. The art of connection between Sinamics S and HMI is shown in the small attachment. AttachmentD:\temp\Direct_access_HMI_WINCCFlexible_EN.pdf (194 Downloads) |
Last edited by: TechTeam at: 2/18/2013 11:22 AMWith best regards, |
|
2/19/2013 11:48 AM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, You can use Ethernet or Profibus - both systems are posssible. For such a configuration you need Simatic Manager, an HMI enginiering system (like WINCC Flexible 2008) and of course Starter to make the commisioning of the Sinamics. In the attachment i have a very small testproject with S7-300, HMI and Sinamics S110. Its just a small example so you can have a look at wiring / simple configuration. AttachmentD:\temp\S110_demokoffer_PN.zip (120 Downloads) |
With best regards, |
|
2/21/2013 3:40 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, You can make a commissioning of a Sinamics (changing parameters etc.) using Starter. For a working DP / PN communication you need the Simatic Manager to create at least a hardware configuration for your S7-PLC. And for your HMI you need the necessary enginiering tool to create HMI Pictures etc. For further informations you can have a look in the function manuals listed here: http://support.automation.siemens.com/WW/view/en/10803928/133300 http://support.automation.siemens.com/WW/view/en/37217116/133300 |
With best regards, |
|
2/22/2013 2:08 AM | |
Posts: 20 Rating: (0) |
okay,thank you very much.. |
Follow us on