Industry Online Support
Technical Forum
6/20/2010 8:41 AM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
In AC Coils, there willbe inductunce pf coil which will produce back emf which limit the current. For DC, there is no such back EMF so only way to limit current is resistance. To increase Resistanc, there are more turns than in AC Please refer following for more detail explanation http://cr4.globalspec.com/thread/8100/AC-relays-versus-DC-relays Hope I was able to provide information you wanted Regards, Devesh |
Last edited by: Vithani at: 6/20/2010 12:27 PMu can give star if you like my answer ;) I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to1 thankful Users |