6/19/2013 7:25 PM | |
Posts: 11 Rating: (0) |
Dear all, I have now set the Profinet IO on starter. As shown in the Joined Document I have Set : - Speed order - Status, Speed, and current measure. To set this configuration I'm using starter connected on X127 Port of the CU320-2-PN Now, I need to set configuration on software who's composed Simatic Net. For that I have Connect Ethernet on X150-P1 Port of the CU320-2-PN. Is is correct to change port after Set Profinet on Starter ? Like shown in the next joined file, I'm trying to configure with NCM PC the connection between My computer and the the 3 S120 throught the CU320-PN. Does anybody have an example who's explain what are the setting to do for that ? Does I need the IP adress of the CU320-PN connected on X150-P1 ? (Default value ?) Is it correct to use OPC, Application and IE Station on NCM Configuration ? All example that I have found use generaly PLC. But in my case I Haven't. I have only a computer connected directly into the CU320-PN Thanks for your help. Regards AttachmentStarter_Conf_IO_Profinet.pdf (406 Downloads) |
6/20/2013 6:44 AM | |
Posts: 319 Rating: (9) |
Even i am looking for this type of example. Direct Communication between Servo and PC. |
6/20/2013 12:40 PM | |
Posts: 11 Rating: (0) |
Dear all, Yesterday I wasn't able to bluild my Profinet network, because I haven't S120 CU 320 GSD File. I download it, and It appear on library. I have build the profinet net network has chown on joined File. Not able for the moment to know if setting are correct ? If I Try to import the NCM setting into Station Configurator Editor, I have error "The configured component with address XXX.XXX.XXX.XXX could not be matched with an existing component". I don't understand why this errorappear... Where is my error setting ? Thanks very much for your help. AttachmentConfig_NCM.pdf (248 Downloads) |
Last edited by: BENY_AKIRA at: 6/20/2013 2:27 PM |
|
Follow us on