7/7/2010 3:36 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello Len, Look at How to Measure and Monitor Temperature with a Pt100 Resistance Temperature Detector (Tip 36) Use the same logic like in "Message 2" and "Message 3" but instead to send the bit to the TD200 which will activate the message send it directly to the outputs Q... Best regards, Hristo Mihalev |
This contribution was helpful to1 thankful Users |
Follow us on