7/9/2018 5:29 PM | |
Joined: 10/5/2014 Last visit: 8/8/2024 Posts: 50 Rating: (0) |
Hi All, I am facing an issue while downloading changes to AS. When ever i try to download changes after changing the interface of SFC like adding/deleting SFC setpoint, the system is not allowing me do changes download. The download gets interrupted saying "Conversion error". The only work around is full download. I have attached the log file generated during this issue. Have anyone faced this issue before...? Thanks, Raja Vijay R AttachmentConversion_error.txt (37 Downloads) |
Follow us on