4/5/2013 8:02 AM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello luciferC4, Have a look at this - How can you group separate signals (variables of the "Bool" data type) to one variable of the "Word" type and again extract them from that "Word" variable (Bool - Word data type conversion)? Hope this helps. |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
4/5/2013 8:20 AM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Not sure if this can help you exactly - but this is another way of overlapping tags How do you program the overlapping of tags with the keyword "AT" in the TIA Portal V11? |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
4/5/2013 11:33 AM | |
Joined: 1/25/2006 Last visit: 2/9/2023 Posts: 257 Rating: (60) |
It is useful links, but this conversion I need to do in Wincc V11 Professional. Not in Step 7. Best regards. |
4/5/2013 2:48 PM | |
Joined: 1/25/2006 Last visit: 2/9/2023 Posts: 257 Rating: (60) |
Hello Ganes10, I use S7 1200 and S7 300 PLCs. Yes, I want use that only in Wincc V11, in this project...
|
4/8/2013 4:57 PM | |
Posts: 3037 Rating: (192)
|
Hello luciferC4, These links are for TIA Portal V11. How in STEP 7 V11 can you access the unstructured data types bit-by-bit, byte-by-byte or word-by-word and symbolically? How do you program the overlapping of tags with the keyword "AT" in the TIA Portal V11? Tweety |
1/29/2016 12:52 PM | |
Joined: 7/24/2014 Last visit: 12/4/2023 Posts: 392 Rating: (66) |
Hello Lucifer, I am facing the problem such that for the 16 bits declared in the PLC needs to be edited in SCADA so to save the number of tags i need to declare it as a whole complete word so i have developed the following script please find the attachment and also how to use it Smit Shah Rate it if you find it helpfull Attachmentscript_smit.rar (427 Downloads) |
Thanks and Regards |
|
This contribution was helpful to2 thankful Users |
Follow us on