6/26/2013 10:16 AM | |
Posts: 72 Rating: (2) |
hi, have u done internal (drive) pzd maping in that 100% = 16383 pulse for PLC side. if u get neg.value reverse direction
|
6/26/2013 10:32 AM | |
Posts: 11 Rating: (0) |
Hi, Thanks for reply. I am a new user of Siemens Product. I haven't PLC. Only a compteur who's read data measure througth OPC server. As display on attached file, I have set number of telegram Send/ Read for profinet exchange. I don't understand what is the link between 100 % and pulse. Thanks AttachmentConf.pdf (221 Downloads) |
6/26/2013 10:38 AM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi Data Type of p2000 is Floating (also that of r63) so you need to read the value as 32bit long register defined as REAL. Attached file is for your reference. Regards, Manmeet.
AttachmentP2000.pdf (352 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on