10/21/2019 2:36 PM | |
Posts: 6 Rating: (0) |
Hi ! Beeing pretty new her and not really a programmer I wondered if anyone here could help out The attached program works fine on LOGO 6,but somehow the Analog input reacjts more like a digital one The unit is a LOGO 8, 6ED 1052-1MD08-0BA0 Input 1 and 2 signal from incremental encoder Input 3 and 4 min and max sensor And input 7 0-10 Vdc (pot. meter) Output 1-4 turns a motor CW or CCW Program is supposed to turn motor depending on pot meter setting Very long story, hope it makes some sense And thanks in advance AttachmentCircuit Diagram1_06_M65.zip (113 Downloads) |
Last edited by: finn_logo at: 10/22/2019 07:06:09 |
|
10/21/2019 2:39 PM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200)
|
Pleas be so kind and upload the LSC diagram as a ZIP file. Thanks. |
10/22/2019 7:06 AM | |
Posts: 6 Rating: (0) |
Program uploaded as .zip-file |
10/22/2019 8:27 AM | |
Joined: 12/18/2014 Last visit: 9/20/2024 Posts: 33807 Rating: (4200)
|
Attached a screen video. I downloaded the program, pulled the upper blocks slightly apart (so I can look better), set the hardware selection to LOGO! 8.FS4 and then transferred the program to my FS4. AttachmentOnline_test.zip (97 Downloads) |
This contribution was helpful to1 thankful Users |
10/22/2019 12:35 PM | |
Posts: 6 Rating: (0) |
Thanks for your effort I will keep searching |
10/22/2019 1:48 PM | |
Posts: 6 Rating: (0) |
Hi Scorp - and thanks for wacthing ! As I wrote, I'm not a trained programmer So I have actually just loaded the program and used with the OBA6 Now they are hard to get, so we swap to the new OBA8, and we got the problem The program was uploaded from the LOGO Here is the original program - if that makes any sense AttachmentM65_Probeklappe_Inkrementalgeber.zip (94 Downloads) |
Follow us on