2/25/2014 8:05 AM | |
Joined: 5/27/2012 Last visit: 6/26/2024 Posts: 177 Rating: (0) |
Hi.A problem is solved.I change a type of value on a buttonF8 on the screen 17 an transfer was done.Now all OK.Very thanks to guyMarcjanfor helping about F8.But intresting same project on a Protool work without problem with a old value. The forum is great.
|
This contribution was helpful to2 thankful Users |
2/25/2014 8:45 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715) |
Hello, The project does not compile because of the error with F8. I have attached a new project, compiles and runs without error. You have to check the F8 function (New-start-homing), in the ZIP is a document with the corrected error. I see you found it already, I had these kind of problems with conversion before, you are lucky it's only one button and there was an error report regards, Marcjan Attachmentop177B.zip (132 Downloads) |
Last edited by: Marcjan at: 2/25/2014 8:50 AMProblem solved? |
|
This contribution was helpful to1 thankful Users |
Follow us on