6/5/2011 12:03 PM | |
Posts: 691 Rating: (37) |
The program can be uploaded to the Engineering PC having Siemens Softwares If its PLC then Step 7 will be sufficient. |
6/5/2011 4:13 PM | |
Joined: 10/7/2005 Last visit: 9/20/2024 Posts: 3021 Rating: (1054)
|
But what if Udara wants to make sure that he has the latest actual DB values backed up on the MMC? In that case "Copy RAM to ROM" is actually quite useful and moreinfo on all things related to this can be found in the FAQ below: What is the effect of the STEP 7 function "Copy RAM to ROM"? @Udara: As for your orignal question, I'm afraid I can't tell you if "Copy RAM to ROM" will work when the PLC is password protected (never tried it and don't have a CPU handy right now to test it). I'd say simply give it a try (it either works or it doesn't) and let us know what the result is. I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on