11/12/2018 6:00 PM | |
Posts: 64 Rating: (7) |
Hi jabbi_king, I think you need to install the configuration software from here. then you should follow the 'getting started' guide for the function module here. I have attached an example configuration in HW Config. I hope this can help you towards a solution |
Last edited by: Jen_Moderator at: 11/13/2018 10:16:15 AMOptimized links. |
|
11/22/2018 10:39 AM | |
Joined: 1/26/2014 Last visit: 3/19/2024 Posts: 164 Rating: (0) |
Diagnostic buffer for CPU 416-3 is attached also |
11/22/2018 12:28 PM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi jabbi_king, the error message of the diagnostic buffer means, that the CPU can't read the parameter from the FM 350-1 modul. Which Version of configuration software do you have installed? with regards |
11/22/2018 1:40 PM | |
Joined: 1/26/2014 Last visit: 3/19/2024 Posts: 164 Rating: (0) |
Dear Heisenberg2 I have installed FM-ConfigPackage_V102_SE. Because my hardware has v1.0.2 |
Follow us on