Industry Online Support
Technical Forum
8/5/2014 9:53 AM | |
Joined: 8/1/2014 Last visit: 1/31/2023 Posts: 12 Rating: (1) |
@eisenpferdreiter: i have 1pulse/m3, i don't have maximum flow, the flowmeter runs continously. The flowmeter will be connected directly to the I0.0 on the S7-1200. @William B.: are two different projects. My hardware is S7-1200 1212C AC/DC/RLY. |
8/5/2014 2:39 PM | |
Joined: 7/7/2010 Last visit: 4/24/2024 Posts: 14624 Rating: (2348)
|
With the RLY outputs, you cannot output as fast as the input can pulse, so add a signal board with a DC output to use for our input follower. That solves I0.0 to Qx.0 follower need. The other is to create a frequency rather than counter- assuming it is counting fast enough to not be in the "noise" level. Convert the frequency to m^3/sec for flow rate. Just be sure to put your input filtering low enough to handle the expected range of the inputs at the fastest rates. |
science guy |
|
Follow us on