8/2/2007 4:25 PM | |
Posts: 5822 Rating: (412) |
Dear Regardt, I think the Communication Forum would be the right one for you, but I inform the Moderator to switch this question. J_Bell |
8/3/2007 9:53 AM | |
Posts: 2 Rating: (0) |
Hi J_Bell Thanks for the reply I think this is the version info for Simatic Net (SIMATIC NET S7-1613 2006). Here's also more info about the dll's used and the Simatic Net Configuration App. Dll's used : OpcRcw.Da (3.0.2.2),OpcRcw.Comn (1.10.1.20) Simatic Net Configuration application version : SIMATIC NET Konfiguration Version: V6.4 Thanks Regardt |
8/3/2007 10:53 AM | |
Posts: 5822 Rating: (412) |
Dear Regardt, such a behavior is not known to me. Sadly it is very hard to figure out such a situation in the Forum. I would recommend contacting the Customer Support with the following Information’s: |