6/8/2011 3:41 PM | |
Joined: 10/7/2005 Last visit: 9/20/2024 Posts: 3021 Rating: (1054)
|
Hello ssantiago, hello Tala it appears that there is a mismatch concerning the CP342-5 DP Slaves I/O config that theDP Master expects to "see" (done in HWconfig of the DP master CPU) and the one that is actually configured for the CP342-5 (done via the setup of DP_Send/DP_RECV calls and related DB's). Its hard to say what is exactly wrong without looking at your S7 projects (pelase upload them). For now I adda couple oflinks which have more on the matter and there's plenty more info to be found on the subject of CP342-5 with a search at https://support.automation.siemens.com: What are the differences between an integrated DP interface of my CPU (e.g. CPU 315-2 DP) and the DP interface of the CP 342-5? What master/slave communication options are available on PROFIBUS DP? I hope this helps |
Cheers |
|
6/8/2011 9:05 PM | |
Posts: 20 Rating: (0) |
Attached is the program of Salve Node connested with CP 342-5, please chwck wether the configuration is correct or not, the Bus Fault is blinking on the CP 342-5. the profibus address is 5 in the CP 342-5 but in the HMI it shows profibus DP address = 100, there is one screen which shows the profibus address. I downloaded the HW configuration several times but its still showing hundred there but when I upload the program from the PLC it shows me the Profibus Address of CP 342-5 = 5, The Diagnostic Buffer is syaing that the Mastre and Slave configuration mismatch. The Master DP program is attached in the next post.
AttachmentC7_613_CPU_cp324_5_08062011.zip (307 Downloads) |
6/8/2011 9:08 PM | |
Posts: 20 Rating: (0) |
The attached program is the S7 300 Master DP, there are several nodes in the HW configuration the one which is not working is node 5. When I check the Diagnostics of this node its saying that, DP slave not available.
AttachmentS7_300_Master_DP_06082011.zip (299 Downloads) |
Follow us on