2/24/2010 11:52 PM | |
Posts: 5 Rating: (0) |
Thak you for your reply mate, Find attached more informations about that case, and please check the questions that it contains. If I get the answers it will help me a lot regards, Nairo AttachmentCase.pdf (108 Downloads) |
3/2/2010 9:21 AM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8615 Rating: (1147) |
Hi, When you use CP342-5, you can not use SFC14 and SFC15 You will have to use FC1 and FC2 (DP_send and DP_RECV) Also have a look at: What you should watch out for when configuring a CP342-5 as DP-master? Edit: See also this link: What are the differences between the integrated DP interface of a CPU (e.g. CPU315-2DP) and the DP interface of the CP342-5? Best regards, Wizard |
Last edited by: Wizard at: 3/2/2010 9:23 AM |
|
This contribution was helpful to1 thankful Users |