3/16/2017 2:59 PM | |
Joined: 10/18/2006 Last visit: 2/9/2024 Posts: 120 Rating: (15) |
Although the post is a bit outdated, the black plane connection between the CPU and the CP is the bottle neck. It is just 187,5 kBit/s! So it doesn't matter if you use an external CP343-1 or the MPI interface, the performance is the same. The only way to have better performance with S7-300 CPU is using the internal Ethernet / PROFINET interface on the CPU. If doing so, expect update cycle less 10ms. |
iba AG - Data Acquisition and Analysis the way it should be |
|
Follow us on