6/14/2011 8:38 PM | |||
Joined: 6/14/2011 Last visit: 4/15/2024 Posts: 2 Rating: (0) |
Is it possible to use CP 5711 for direct transfer WinCC flexible project from the PC to the Windows-based panel (TP 270)? I only find this: Notes on the USB PC adapter (6ES7972-0CB20-0XA0)
best regards |
||
6/14/2011 8:56 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181)
|
Hello, So, for sure PC Adapter is not released for the transfer. Check it there - What transfer options are available in the various operator panels? But CP5711 should works. Follow these steps How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? <OFFTOPIC> How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this? Best regards, Hristo Mihalev |