11/28/2015 8:27 AM | |
Posts: 1 Rating: (0) |
hi i installed pcs7 v8.1 on both of them. pcs7 has installed on dl320e without problem and cp1623 worked properly and the software(pc/pg interface known it) but i install pcs7 8.1 on dl380 after setup finished i rebooted my pc when windows run it could recognize cp1623 but after a few minute error happened cp1623(1):an internal error occurred there are port pcie 3.0 x8 and x16 on both but on one of working without problem but on another one work with error how could i fix it ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/30/2015 1:39:43 PMNew subject after splitting |
|
6/16/2016 9:09 PM | |
Joined: 2/6/2008 Last visit: 2/25/2023 Posts: 1 Rating: (0) |
Hello, We are facing the same issue. Were you able to solve this problem? Thanks. |
7/20/2016 8:22 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4776 Rating: (123) |
New question published by RenatoAlex is split to a separate thread with the subject CP1623, CODE 31. Best regards |
3/9/2017 6:56 PM | |||||||||||||
Joined: 11/20/2013 Last visit: 2/29/2024 Posts: 25 Rating: (1) |
Hello Everyone All new HP DL380 Gen9 Server/other servers(maybe) need to downgrade to Bios V1.4 for detection of CP-1623. Online ROM Flash Component for Windows x64 - HP ProLiant DL380 Gen9/DL360 Gen9 (P89) Servers
http://h20566.www2.hpe.com/hpsc/swd/public/detail?swItemId=MTX_8123c9e1d3b74f5c99c5bf3ed3 This helped me to make the detection of CP1623 possible. |
||||||||||||
Follow us on