3/3/2007 2:09 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Hi, You have to use PROFIBUS FDL whereby you can work with FC5 "AG_SEND" {V4.2} and FC6 "AG_RECV"{V4.7} (from the communication library "SIMATIC_NET_CP"). In Netpro please make some FDL connections, if you have all CPU's in one project then it is no problem. Load all software, hardware and Netpro and your ready. See also in "Application & Tools" the examplewith download for a FDL connection between a S&-300 and a S7-400: FDL communication with SDA service via PROFIBUS CPs and Send/Receive interface |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on