Industry Online Support
Technical Forum
7/9/2007 1:49 PM | |
Posts: 25 Rating: (0) |
Thank u Danielle, How do u make a delta load from your ES to the OS? (In the Simatic Manager?) Which settings needs to be made for this? |
7/9/2007 2:18 PM | |
Posts: 1275 Rating: (123)
|
Hi Riaz, The Load Online Changes is a function which allows you to configure changes in the ES, and load them into the OS, while it's still in runtime. With it, runtmie doesn't need to be stopped. You can see some more info on it here. Beware that it has limitations. Not all functions are supported. If you access some configurations in WinCC, such as the Parameters tab, under Computer, you'll get the message: "This configuration will disable the DeltaLoader support....". This message means that if you change anything there the Load Onilne Changes function will not see that, and this change will not be made in the OS. Some time ago I put together a .doc with instructions ( a little manual), and another with the limitations from load Online Changes. The manual is in Portuguese, but the limitations are in English, as copied from the WinCC documentation. I've attached it for you. Best regards, Danielle AttachmentRestrictions for Load Online Changes.pdf (103 Downloads) |
Follow us on