4/28/2013 5:58 PM | |
Joined: 4/27/2013 Last visit: 6/30/2023 Posts: 5 Rating: (0) |
Thanks for the reply. I have already installed the HSPs including 0026. The TIA Portal seems to be communicating with the CPU but just keeps indicating that it is not compatible with the CPU selected in the project. I am at a loss to understand what's wrong. TIA Portal seems to be talking to the CPU but it thinks it's the wrong type but it is the same part number. The only difference that I can see is that the firmware in the TIA selected CPU is 3.0 and the connected CPU is 3.0.2. However, 3.0.2 cannot be selected in TIA Portal whether the CPU is selected from the hardware list or is detected by TIA Portal. I've also tried to reset to factory settings using the Primary Setup Tool but although it seems to see the CPU it just reports that the factory reset can't be carried out in its current operating mode. I assume it's in stop, the Run/Stop LED is lit yellow all the time. |
4/28/2013 9:05 PM | |
Joined: 8/1/2012 Last visit: 7/30/2023 Posts: 178 Rating: (15) |
[quote user="SteveJG"]Thanks for the reply. I have already installed the HSPs including 0026. The TIA Portal seems to be communicating with the CPU but just keeps indicating that it is not compatible with the CPU selected in the project. I am at a loss to understand what's wrong. TIA Portal seems to be talking to the CPU but it thinks it's the wrong type but it is the same part number. The only difference that I can see is that the firmware in the TIA selected CPU is 3.0 and the connected CPU is 3.0.2. However, 3.0.2 cannot be selected in TIA Portal whether the CPU is selected from the hardware list or is detected by TIA Portal. I've also tried to reset to factory settings using the Primary Setup Tool but although it seems to see the CPU it just reports that the factory reset can't be carried out in its current operating mode. I assume it's in stop, the Run/Stop LED is lit yellow all the time. Hello Do you use any additional softwares installed on your windows that has relation with your network or internet connection?? I have exactly the same problem as you , when I use " Proxifire ". This software changes my network configuration. |
|
|
4/29/2013 8:57 AM | |
Posts: 4 Rating: (0) |
Once I had the same problem. I did the following: Click on 'Online' ---> 'Accessible devices'. Step 7 TIA portal will connect with the plc and assigne a new IP automaticaly. |
7/25/2013 8:29 AM | |
Posts: 23 Rating: (0) |
Dear expert, I've the same problem, can not connect to CPU1214 V3 (i'm using TIA Pro V12-Update 3). I tried to use S71200 tool (S7-1200 Tool - 2.0.0.5) to detect IP or Mac Add PLC but i can not connect. Have any one have solution, please help me. Best regards, DangNhutHien |
7/25/2013 5:30 PM | |
Joined: 8/1/2012 Last visit: 7/30/2023 Posts: 178 Rating: (15) |
Hi can you see the CPU in project tree/online access ?? |
|
|
7/25/2013 7:49 PM | |
Posts: 23 Rating: (0) |
Dear Mr Mo.Sa, Online access is imposible, cannot detect CPU. With firmware V2 i connect still alright but with firmware V3, i can not please help me Best regards, DangNhutHien |
4/8/2014 11:49 PM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
|
My Forum is the place to personalize your profile, |
|
Follow us on